PE_low_level_init.h

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PE_low_level_init.h

2,268件の閲覧回数
MToM
Contributor I

Hello,

 

I created a Kinetis 1.3.0 project with processor expert. The build failed with error: /Static_Code/System/PE_low_level_init.c:51:31: fatal error: PE_low_level_init.h: No such file or directory

 

pls Help

Thomas

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,792件の閲覧回数
niconico
Contributor I

Hi MToM,

 

I was having the same issue and I solve it changing the Project Location. It seems that KIDS can't handle some characters ("ñ" in my case). To be sure I also used a really short route.

Hope it helps.

Have a great day.

 

Nicolás.

0 件の賞賛
返信

1,792件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Thomas,

Please make sure to generate the Processor Expert code before building the project:

pastedImage_1.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信