PE_low_level_init.h

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PE_low_level_init.h

2,280 次查看
MToM
Contributor I

Hello,

 

I created a Kinetis 1.3.0 project with processor expert. The build failed with error: /Static_Code/System/PE_low_level_init.c:51:31: fatal error: PE_low_level_init.h: No such file or directory

 

pls Help

Thomas

标签 (1)
0 项奖励
回复
2 回复数

1,804 次查看
niconico
Contributor I

Hi MToM,

 

I was having the same issue and I solve it changing the Project Location. It seems that KIDS can't handle some characters ("ñ" in my case). To be sure I also used a really short route.

Hope it helps.

Have a great day.

 

Nicolás.

0 项奖励
回复

1,804 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Thomas,

Please make sure to generate the Processor Expert code before building the project:

pastedImage_1.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复