Nothing shows up for Port in the Debug Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nothing shows up for Port in the Debug Configuration

1,901 Views
ylee
Contributor II

I have been using FRDM-KL25Z with the KDS 1.0.1 and updated KDS to 1.1.1 two days ago.

 

Ever since, even though the debug driver and OpenSDA ports are installed as shown in the following picture, I do not have the port when I tried to set Debug Configuration.

 

Does anyone know what is happening? I have been pulling my hair for two days now....

15732_15732.png10-16-2014 9-17-49 AM.png

15735_15735.png10-16-2014 9-26-38 AM.png

Labels (1)
0 Kudos
Reply
3 Replies

1,810 Views
BlackNight
NXP Employee
NXP Employee

Your drivers look ok, I have:

pastedImage_0.png

Did you press the 'Refresh' button in that dialog?

Erich

0 Kudos
Reply

1,810 Views
ylee
Contributor II

Yes, I tried several times. Even rebooting, uninstalling and re-installing all the drivers and software did not solve the issue. :smileysad: Thanks for your reply though.

0 Kudos
Reply

1,810 Views
BlackNight
NXP Employee
NXP Employee

A student approached me several days ago with the same problem (Windows 8, if this matters) and USB 3.0. Changing to a USB 2.0 port helped. Not sure if USB 3.0 is a problem on your side.

You say you re-installed the drivers? Did you remove them from the device manager?

What might be an alternative route if you try the Segger J-Link driver for the FRDM-KL25Z? See http://mcuoneclipse.com/2013/05/16/freedom-board-with-segger-opensda-debug-firmware/

Erich

0 Kudos
Reply