Not able to debug FRDM KL46z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to debug FRDM KL46z

1,990件の閲覧回数
juanignaciotroi
Contributor III

Hello

I am trying to debug with the FRDM KL46z. As a first attempt, I'm trying to run the "hello_world" example, which provides the KSDK. I have followed exactly all the instructions mentioned on FRDM getting started steps (FRDM-KL46Z|Freedom Development Platform|Kinetis MCU|NXP ) and after realising that that one doesn't work, I have also tryed with the "Getting Started with Kinetis SDK (KSDK) v.1.3", that is provided with the KSDK. However, this last one hasn't solved my problem either. 

When trying to debug, the following error turns up in the KDS console:

Open On-Chip Debugger 0.8.0-dev (2015-01-09-16:22)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Info : only one transport option; autoselect 'cmsis-dap'
Error: unable to open CMSIS-DAP device
Error: unable to init CMSIS-DAP driver
Error: Error selecting 'cmsis-dap' as transport
Runtime Error: C:/Freescale/KDS_v3/openocd/bin/..//scripts/kinetis.cfg:3:
in procedure 'script'
at file "embedded:startup.tcl", line 58
in procedure 'interface' called at file "C:/Freescale/KDS_v3/openocd/bin/..//scripts/kinetis.cfg", line 3

I have read one forum where it is said that the FRDM KL46z firmware doesn't work on OS Win 8.1. Is this true? Has anybody had a similar problem?

Kind regards, 

Juan Ignacio Troisi

タグ(2)
0 件の賞賛
返信
1 返信

1,706件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello

The same question with this thread  https://community.nxp.com/message/915191 

BR

Alice

0 件の賞賛
返信