No repository found containing: binary,com.somniumtech.kds.executable.gtk.linux.x86,0.0.0.201407291534

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No repository found containing: binary,com.somniumtech.kds.executable.gtk.linux.x86,0.0.0.201407291534

ソリューションへジャンプ
3,140件の閲覧回数
leechakkhiam
Contributor II

Installing software encounter the following error. "No repository found containing: binary,com.somniumtech.kds.executable.gtk.linux.x86,0.0.0.201407291534"

How to fix it?

Thank You.

ラベル(1)
1 解決策
2,683件の閲覧回数
g5pw
Contributor I

This has been solved, launch eclipse as root and install the update, then you can continue using it normally. See here: Eclipse Update install problem | Freescale Community

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,684件の閲覧回数
g5pw
Contributor I

This has been solved, launch eclipse as root and install the update, then you can continue using it normally. See here: Eclipse Update install problem | Freescale Community

0 件の賞賛
返信
2,683件の閲覧回数
leechakkhiam
Contributor II

Thank you. This solve the problems.

0 件の賞賛
返信
2,683件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Lee,

what's your system platform? version?

0 件の賞賛
返信
2,683件の閲覧回数
leechakkhiam
Contributor II

Hi ZhangJennie:

I am using 32bit xubuntu 14.04.

Thank you.

0 件の賞賛
返信
2,683件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Lee,

Sorry little late with my feedback.

See you've solved the problem.

On my side I'm able to create an build a project created with the project wizard for FRDM-K64F.

My configuration is:

  - Win 7 32 OS,

  - VirtualBox,

  - Ubuntu 14.04.1 (ubuntu-14.04.1-desktop-i386.iso)

  - KDS V1.1.0.

After to have installed the tool as root, the tool must be launch as root too:

  sudo /opt/Freescale/KDS_1.1.0/eclipse/kinetis-design-studio


This is working fine on my side.

Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------