No repository found containing: binary,com.somniumtech.kds.executable.gtk.linux.x86,0.0.0.201407291534

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No repository found containing: binary,com.somniumtech.kds.executable.gtk.linux.x86,0.0.0.201407291534

Jump to solution
3,293 Views
leechakkhiam
Contributor II

Installing software encounter the following error. "No repository found containing: binary,com.somniumtech.kds.executable.gtk.linux.x86,0.0.0.201407291534"

How to fix it?

Thank You.

Labels (1)
1 Solution
2,836 Views
g5pw
Contributor I

This has been solved, launch eclipse as root and install the update, then you can continue using it normally. See here: Eclipse Update install problem | Freescale Community

View solution in original post

0 Kudos
Reply
5 Replies
2,837 Views
g5pw
Contributor I

This has been solved, launch eclipse as root and install the update, then you can continue using it normally. See here: Eclipse Update install problem | Freescale Community

0 Kudos
Reply
2,836 Views
leechakkhiam
Contributor II

Thank you. This solve the problems.

0 Kudos
Reply
2,836 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Lee,

what's your system platform? version?

0 Kudos
Reply
2,836 Views
leechakkhiam
Contributor II

Hi ZhangJennie:

I am using 32bit xubuntu 14.04.

Thank you.

0 Kudos
Reply
2,836 Views
trytohelp
NXP Employee
NXP Employee

Hi Lee,

Sorry little late with my feedback.

See you've solved the problem.

On my side I'm able to create an build a project created with the project wizard for FRDM-K64F.

My configuration is:

  - Win 7 32 OS,

  - VirtualBox,

  - Ubuntu 14.04.1 (ubuntu-14.04.1-desktop-i386.iso)

  - KDS V1.1.0.

After to have installed the tool as root, the tool must be launch as root too:

  sudo /opt/Freescale/KDS_1.1.0/eclipse/kinetis-design-studio


This is working fine on my side.

Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------