Multiple instances KDS to debug two Freedom Boards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple instances KDS to debug two Freedom Boards

1,803 Views
carloshass
Contributor II

WhtHello!

 

I'm trying to use 2 KDS on same machine, to develop a CANbus network.

 

I've 2 FRDM-KE06Z boards, configured 2 workspaces.

 

The started both KDS, each in a workspace.

 

Then i configured first KDS to debug with one of the KE06Z boards, configured on debug configurations, start, all right:

 

90251_90251.pngpastedImage_2.png

 

Then i changed to another KDS instance, configured debug to the another KE06Z board:

 

90252_90252.pngpastedImage_3.png

 

Each debug separately is working, but, when i tryed to debug one, and then debug another, i got this error:

 

90253_90253.pngpastedImage_4.png

 

I'm missing some configuration?

 

 

Regards,

CH

Labels (1)
0 Kudos
Reply
2 Replies

1,596 Views
DavidS
NXP Employee
NXP Employee

Hi CH,

I have tried and failed when having two KDS sessions opened to debug two Freedom boards as well.

My workaround is to have one Freedom board use PEMicro OpenSDA and the other board to use Segger JLink firmware.

Regards,

David

0 Kudos
Reply

1,596 Views
BlackNight
NXP Employee
NXP Employee

I'm able to debug multiple boards in parallel with the Segger firmware, see Debug Multiple Boards with GDB at the Same Time | MCU on Eclipse

I have not yet able to do the same with the P&E Multilink/OpenSDA firmware.

Erich

0 Kudos
Reply