Multiple instances KDS to debug two Freedom Boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple instances KDS to debug two Freedom Boards

1,789件の閲覧回数
carloshass
Contributor II

WhtHello!

 

I'm trying to use 2 KDS on same machine, to develop a CANbus network.

 

I've 2 FRDM-KE06Z boards, configured 2 workspaces.

 

The started both KDS, each in a workspace.

 

Then i configured first KDS to debug with one of the KE06Z boards, configured on debug configurations, start, all right:

 

90251_90251.pngpastedImage_2.png

 

Then i changed to another KDS instance, configured debug to the another KE06Z board:

 

90252_90252.pngpastedImage_3.png

 

Each debug separately is working, but, when i tryed to debug one, and then debug another, i got this error:

 

90253_90253.pngpastedImage_4.png

 

I'm missing some configuration?

 

 

Regards,

CH

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,582件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi CH,

I have tried and failed when having two KDS sessions opened to debug two Freedom boards as well.

My workaround is to have one Freedom board use PEMicro OpenSDA and the other board to use Segger JLink firmware.

Regards,

David

0 件の賞賛
返信

1,582件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I'm able to debug multiple boards in parallel with the Segger firmware, see Debug Multiple Boards with GDB at the Same Time | MCU on Eclipse

I have not yet able to do the same with the P&E Multilink/OpenSDA firmware.

Erich

0 件の賞賛
返信