MKL17Z - How to initialize user flash data at compile time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL17Z - How to initialize user flash data at compile time

1,638 Views
sys
Contributor III

Hi all,

 

I'm using MKL17Z256VFM4 with KDS 3.0.0. I would like to know if there is a way to put default values in the flash user block at compile time.

For understanding, I would like to do like I do with CodeWarrior 6.x with the "@" directive, for example:

 

const uint EEDefault[2] @ 0xE000 = {

  0x0001,

  0x0002

}

 

In this way I'm sure that after downloaded the executable, in the address 0xE000 I have the value 0x0001, and so on.

 

Is it possibile to do stuff like this with KDS and MKL17Z in similar way? I know it's not possibile with MKE02Z, but these two micro are quite different, so maybe there is a way with MKL17Z?

It would be good, so I dont need to make my own init-flash for every project.

 

Thanks in advance!

Sandro

Labels (1)
2 Replies

1,417 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Sandro,

Please take a look to the following document, it explains how to place code and data in specific ROM and RAM addresses:

Relocating Code and Data Using the KDS GCC Linker File for Kinetis

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,417 Views
sys
Contributor III

Hello Carlos,

thanks for the answer, I will take a look soon and let you know!

Thank you,

Best Regards,

Sandro