Kinetis design studio MKE1xF support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis design studio MKE1xF support

ソリューションへジャンプ
1,722件の閲覧回数
michaelheidinge
Contributor III

The new Kinetis devices MKE1xF look promising for me.

Is there a way to get them supported with Kinetis Design Studio?

As far as I see, they are not yet on the list for supported devices with KDS 3.2.

 

Apprichiating your support,

-Michael

ラベル(1)
0 件の賞賛
返信
1 解決策
1,361件の閲覧回数
MarekTrmac
NXP Employee
NXP Employee

Hi Michael,

download SDK 2.x from https://mcuxpresso.nxp.com/

Then use File - New - Kinetis SDK 2.x Project to create new project for that device.

I recommend to update NewProjectWizard from KDS update site, if you have not done yet.

Regards

Marek

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,362件の閲覧回数
MarekTrmac
NXP Employee
NXP Employee

Hi Michael,

download SDK 2.x from https://mcuxpresso.nxp.com/

Then use File - New - Kinetis SDK 2.x Project to create new project for that device.

I recommend to update NewProjectWizard from KDS update site, if you have not done yet.

Regards

Marek

0 件の賞賛
返信