Kinetis KwikStik

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis KwikStik

1,120件の閲覧回数
lijofrancis
Contributor III

Dear sir,

              We buy board Kinetis KwikStik(k40) Board.I found problem is that the connector pin out PTE7 (B21) in user"s manual not the same pin.It is actually PTE11.please check any further change

ラベル(1)
0 件の賞賛
返信
1 返信

981件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Lijo Francis,

I attached you the explanation for your answer.

http://cache.freescale.com/files/32bit/doc/ref_manual/KWIKSTIKK40UM.pdf?fpsp=1pte7__.png

http://cache.freescale.com/files/32bit/doc/ref_manual/K40P144M100SF2RM.pdf

PTE7_.png

UART5 is a signification (name) on the board, it is not in connection with the chip. The signification (name) on the chip is UART3, so UART3RTS and is pin PTE7.

On port PTE11 is UART5RTS.

Best Regards,

Iva

0 件の賞賛
返信