KV58 S19 file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KV58 S19 file

跳至解决方案
1,288 次查看
a8Chcx
Contributor V

Hi,

I am using "arm-none-eabi-objcopy --srec-len=64 --srec-forceS3 -O srec "aaa.elf"  "aaa.S19"" to generate S19 file.

The generated S19 as follows. At the end of file, it is not 64-bit alignment...

"

...............

S345100301C0000000000000000006D0CF43EBFD4C3E000000000000F03F000000000000F83F000000000000304300000000000030C34300000010000020F8B500BFF8BC08BC69
S315100302009E467047F8B500BFF8BC08BC9E467047BB
S30D100302104402FF7F0100000008
S30910030218250402108E
S3091003021C01040210AE
S34510030220000040010080000000093D00010000000000000000000000000000000000000000000000000000000000000000000000F001031000000000000000000000000079
S33D1003026000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000010000020000000001D
S705100204C91B

"

Because of 64-bit alignment required for KV58, I need to generate S19 file with 64-bit alignment.

Could you tell me how to do it?

Thanks,

Christie

0 项奖励
回复
1 解答
1,167 次查看
BlackNight
NXP Employee
NXP Employee
0 项奖励
回复
2 回复数
1,168 次查看
BlackNight
NXP Employee
NXP Employee
0 项奖励
回复
1,167 次查看
a8Chcx
Contributor V

Thanks. It works...

0 项奖励
回复