KV58 S19 file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,146件の閲覧回数
a8Chcx
Contributor IV

Hi,

I am using "arm-none-eabi-objcopy --srec-len=64 --srec-forceS3 -O srec "aaa.elf"  "aaa.S19"" to generate S19 file.

The generated S19 as follows. At the end of file, it is not 64-bit alignment...

"

...............

S345100301C0000000000000000006D0CF43EBFD4C3E000000000000F03F000000000000F83F000000000000304300000000000030C34300000010000020F8B500BFF8BC08BC69
S315100302009E467047F8B500BFF8BC08BC9E467047BB
S30D100302104402FF7F0100000008
S30910030218250402108E
S3091003021C01040210AE
S34510030220000040010080000000093D00010000000000000000000000000000000000000000000000000000000000000000000000F001031000000000000000000000000079
S33D1003026000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000010000020000000001D
S705100204C91B

"

Because of 64-bit alignment required for KV58, I need to generate S19 file with 64-bit alignment.

Could you tell me how to do it?

Thanks,

Christie

0 件の賞賛
返信
1 解決策
2,025件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信
2 返答(返信)
2,026件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信
2,025件の閲覧回数
a8Chcx
Contributor IV

Thanks. It works...

0 件の賞賛
返信