KSDK-1.1 SPI include file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSDK-1.1 SPI include file

Jump to solution
1,421 Views
oaf
Contributor IV

I'm using KDS-2.0.0 and KSDK-1.1.0.

In my project I use a SPI device, but the PEx generated .h file doesn't contain a full definition of what is needed

 

This is how I do it:

 

#include "spiCom0.h"

 

static int HW_SPI0TxHelper(uint8_t *txBuff, size_t length)

{

    spi_status_t stat = kStatus_SPI_Busy;

    int err = 1;

 

 

    if(SPI_DRV_MasterTransfer(FSL_SPICOM0, NULL, txBuff, NULL, length) == kStatus_Success)

    {

        uint32_t txCnt = 0;

 

        while(stat != kStatus_Success)

        {

            stat = SPI_DRV_MasterGetTransferStatus(FSL_SPICOM0, &txCnt);

        }

 

        if(stat == kStatus_Success)

            err = 0;

    }

 

 

    return err;

}

 

When compiling this sw I got the following error messages:

 

..\..\Project\Infrastructure\HW.c:99:2: error: unknown type name 'spi_status_t'

  spi_status_t stat = kStatus_SPI_Busy;

  ^

..\..\Project\Infrastructure\HW.c:99:22: error: 'kStatus_SPI_Busy' undeclared (first use in this function)

  spi_status_t stat = kStatus_SPI_Busy;

                      ^

 

I thought that the SPI .h file should contain the definition for all that is needed to use the SPI interface?

What is the intended use here (from the design point of view)?

Is this an error, or have I complete misunderstood?

Labels (1)
0 Kudos
Reply
1 Solution
1,191 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Ole,

You can find the SPI interface function under the SPI component , and in the file of "fsl_dspi_master_driver.h" / "fsl_dspi_slave_driver.h" and so on .

Please see the screenshot below :

pastedImage_0.png

Hope it helps

Alice

View solution in original post

0 Kudos
Reply
2 Replies
1,192 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Ole,

You can find the SPI interface function under the SPI component , and in the file of "fsl_dspi_master_driver.h" / "fsl_dspi_slave_driver.h" and so on .

Please see the screenshot below :

pastedImage_0.png

Hope it helps

Alice

0 Kudos
Reply
1,191 Views
oaf
Contributor IV

Well you put me on the track, there is a very significant 'd' which does all the difference.

I have included the fsl_spi_master_driver.h where the correct is fsl_dspi_master_driver.h(!)

If I may suggest a change it will be that the API documentation tells which file to include...

0 Kudos
Reply