KDS-2.0.0 libraries

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS-2.0.0 libraries

1,814件の閲覧回数
oaf
Contributor IV

Hi,

 

When using KDS-2.0.0 on my project at irregular intervals the project will not link!

 

make: *** No rule to make target `E:/Sensors/Modules/HDTransceiver/App/KDS/SDK/lib/gcc/K64F12/output/Debug/platform_lib.a', needed by `HDTR.elf'.  Stop.

make: *** Waiting for unfinished jobs....

 

1. Why doesn't my project know how to make generated code?

2. Even the directory is missing `E:/Sensors/Modules/HDTransceiver/App/KDS/SDK' contains only two directories platform, and rtos

    (so it's not a wonder why it doesn't know how to  make it)

3. So I in panic removed platform_lib.a and startup_lib.a (as my project uses KSDK from precompiled libraries)

4. My project links and works OK

5. On what seems to be random times, the libraries are added back!!! I've not managed to figure out what is triggering this behavior.

 

One genaral comment:

Why is the libraries added on the 'Miscellaneous' tab with full path?

If the 'Libraries' tab was used the libraries could be specified with only name, and the path has not to be repeated,

and as we all know KDS uses a little bit too much on the commandline resulting in various linker problems.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,539件の閲覧回数
oaf
Contributor IV

I've not found any pattern, but it seems that the problem is solved by creating a new project and move all source to the new project.

0 件の賞賛
返信

1,539件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Ole,

do you run a SDK demo code?

can you specify how to reproduce your problem step by step?

Best Regards,

ZhangJun

0 件の賞賛
返信