KDS30 Debug and Prog

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,054件の閲覧回数
CCandido
Contributor V

Hi,

 

KDS20 debug/programming = error, I unistall it.

NOW KDS30 error =;

 

 

 

24810_24810.jpgKDS30_ERRO.jpg

24811_24811.jpgKDS_CONFIGD.jpg

I use Multilink C, conection K22F  ok.

 

How to Configurations for ( Debug and programming flash )?

 

See:

 

Connection from "127.0.0.1" via 127.0.0.1

 

Copyright 2012 P&E Microcomputer Systems,Inc.

 

Command Line :C:\Freescale\KDS_3.0.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.0.8.201504092111\win32\pegdbserver_console -device=Freescale_K2x_K22FX512M12 -startserver -singlesession -serverport=7224 -interface=USBMULTILINK -speed=1000 -usejtag -p

 

 

 

  

 

CMD>RE

 

 

 

  

 

Initializing.

 

Cannot enter background mode. Check connections. 

 

Error Resetting device for programming.

 

 

 

PE-ERROR: Error downloading to the device.

 

thanks.

Carlos.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,840件の閲覧回数
CCandido
Contributor V

hi,

KDS30, IT NOT DEBUG

KDS_INTERFACE_STD.jpg

KDS30 DEBUG AND PROGRAMMER OK.

KDS_INTERFACE_OK.jpg

my programmer it ( P&E Multilink Universal ).

it not run in MODE ( SWD ).

Thanks,

Carlos.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,840件の閲覧回数
takaoyamada
Contributor IV

Greetings,

If you had issues connecting in both KDS2.0 and 3.0, then the issue is most likely in hardware and not in the software.

1) Are you using any custom adapter, custom ribbon cables, external watchdog, a reset circuitry, or other unique hardware?

2) Has this setup worked in the past? Or is this your first attempt? Do you know if the P&E hardware and the board are in working condition?

3) What P&E hardware interface are you using?


Takao YamadaP&E Microcomputer Systems

0 件の賞賛
返信
1,841件の閲覧回数
CCandido
Contributor V

hi,

KDS30, IT NOT DEBUG

KDS_INTERFACE_STD.jpg

KDS30 DEBUG AND PROGRAMMER OK.

KDS_INTERFACE_OK.jpg

my programmer it ( P&E Multilink Universal ).

it not run in MODE ( SWD ).

Thanks,

Carlos.

0 件の賞賛
返信