KDS30 Debug and Prog

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS30 Debug and Prog

Jump to solution
3,223 Views
CCandido
Contributor V

Hi,

 

KDS20 debug/programming = error, I unistall it.

NOW KDS30 error =;

 

 

 

24810_24810.jpgKDS30_ERRO.jpg

24811_24811.jpgKDS_CONFIGD.jpg

I use Multilink C, conection K22F  ok.

 

How to Configurations for ( Debug and programming flash )?

 

See:

 

Connection from "127.0.0.1" via 127.0.0.1

 

Copyright 2012 P&E Microcomputer Systems,Inc.

 

Command Line :C:\Freescale\KDS_3.0.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.0.8.201504092111\win32\pegdbserver_console -device=Freescale_K2x_K22FX512M12 -startserver -singlesession -serverport=7224 -interface=USBMULTILINK -speed=1000 -usejtag -p

 

 

 

  

 

CMD>RE

 

 

 

  

 

Initializing.

 

Cannot enter background mode. Check connections. 

 

Error Resetting device for programming.

 

 

 

PE-ERROR: Error downloading to the device.

 

thanks.

Carlos.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,008 Views
CCandido
Contributor V

hi,

KDS30, IT NOT DEBUG

KDS_INTERFACE_STD.jpg

KDS30 DEBUG AND PROGRAMMER OK.

KDS_INTERFACE_OK.jpg

my programmer it ( P&E Multilink Universal ).

it not run in MODE ( SWD ).

Thanks,

Carlos.

View solution in original post

0 Kudos
Reply
2 Replies
3,008 Views
takaoyamada
Contributor IV

Greetings,

If you had issues connecting in both KDS2.0 and 3.0, then the issue is most likely in hardware and not in the software.

1) Are you using any custom adapter, custom ribbon cables, external watchdog, a reset circuitry, or other unique hardware?

2) Has this setup worked in the past? Or is this your first attempt? Do you know if the P&E hardware and the board are in working condition?

3) What P&E hardware interface are you using?


Takao YamadaP&E Microcomputer Systems

0 Kudos
Reply
3,009 Views
CCandido
Contributor V

hi,

KDS30, IT NOT DEBUG

KDS_INTERFACE_STD.jpg

KDS30 DEBUG AND PROGRAMMER OK.

KDS_INTERFACE_OK.jpg

my programmer it ( P&E Multilink Universal ).

it not run in MODE ( SWD ).

Thanks,

Carlos.

0 Kudos
Reply