KDS2.0.0 does not debug with Windows8 64bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS2.0.0 does not debug with Windows8 64bit

3,602 Views
isaotakashima
Contributor IV

We are making the new project for our product with the following environments.

- FRDM-KE02Z

- KDS 2.0.0

- OpenSDA PEMicro debugger (DEBUG-APP_Pemicro_v106.SDA)

- Windows 8 64bit

 

We can build the code, but we cannot start debugging.

The KDS does not move to debug mode window, please see attached file.

 

Please advise to solve this issue as soon as possible.

 

Best regards,

Takashima

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

3,410 Views
trytohelp
NXP Employee
NXP Employee

Hi,

I don't have the FRDM-KE02Z but a FRDM-KE06Z board.

I've downloaded the FRDM-KE06Z_QSP.zip from our web site.

Similar file is available for this board at the link:

      http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KE02Z&fpsp=1&tab=Design_Tools_Ta...

see to FRDM-KE02Z_QSP: FRDM-KE02Z_QSP Quick Start Package.

After to have loaded the right file on board the OpenSDA was installed and I was able to debug an application on KDS.

Attached you will find a video showing the process.

Do you reproduce the problem with an example created with the wizard ?

      as the example using in the video

Hope this will help you.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,410 Views
trytohelp
NXP Employee
NXP Employee

Hi Isao,

This is just to inform you I will check the problem.

I need to install a Windows 8 OS.

Keep you informed.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply