KDS synthiax error but not true

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS synthiax error but not true

Jump to solution
2,330 Views
pietrodicastri
Senior Contributor II

Good morning

I have a behaviour with KDS.

The editor is outlining as error an expression, but build time no error is present.

This begun to happen since some time, after the same project has correctly worked for months.

 

Suggestions???

 

Thank You

 

138362_138362.pngkdserr.png

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,225 Views
BlackNight
NXP Employee
NXP Employee

Hi Pietro,

maybe I don't see it, but I don't see an error in your screen shot?

As a piece of information: Eclipse is using the 'Indexer' for its internal parsing. So it could be that your Indexer database somehow is not correct. See Fixing the Eclipse Index | MCU on Eclipse .

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
3 Replies
2,226 Views
BlackNight
NXP Employee
NXP Employee

Hi Pietro,

maybe I don't see it, but I don't see an error in your screen shot?

As a piece of information: Eclipse is using the 'Indexer' for its internal parsing. So it could be that your Indexer database somehow is not correct. See Fixing the Eclipse Index | MCU on Eclipse .

I hope this helps,

Erich

0 Kudos
Reply
2,224 Views
pietrodicastri
Senior Contributor II

Yes ,,

Rebuild the index was sufficient,,,

Thank You

0 Kudos
Reply
2,225 Views
trytohelp
NXP Employee
NXP Employee

Hi Pietro,

Can you please provide us a short example reproducing the problem ?

What is the KDS tool version used ?

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply