KDS real time expression missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS real time expression missing

2,619 Views
claudiobrunelli
Contributor II

Hi.

I have to use KDS ide, althouhgt it's not recommended  for new design. 

For some pc problem  I have done a new installation software but now I can not to use the real time expression viewer.

It's very easy to install it, but when I try to show the viewer in the perspective I can not see it. Before, I did these simple operation from menu "Window", "Show view", "Other" and in the PE menu I saw "realTime Expression". Now it's impossible. I have installed, disinstalled, updated but I see only.

Can someone give suggestion ?

Thanks in advance.

Claudio


					
				
			
			
				
			
			
				
			
			
			
			
			
			
		
0 Kudos
Reply
2 Replies

2,449 Views
BlackNight
NXP Employee
NXP Employee

Hi Claudio,

have you updated as well the PEMicro plugin using Help > Install new software using the P&E update site?

pastedImage_1.png

I hope this helps,

Erich

0 Kudos
Reply

2,449 Views
claudiobrunelli
Contributor II

Hi Erich.

Thanks for your assistance.

Yes I have updated the PE plugin. 

But at the beginning, trying to install, I had an error as you can see from attached file named Image_B.

So I re-installed KDS IDE, updated pe plugin and checked again what I had installed. 

I realized that I didn't have the right requirements named P&E Core Plugin 1.2.0 but I have P&E Core Plugin 1.1.43.

May be this the wrong situation (Image_C) ? Can you tell me how I can install P&E Core Plugin 1.2.0 ?

The view of PE that I have (without real time expression) is in Image_D.

Thanks for your suggestion.

Claudio

Immagine_B.pngImmagine_C.pngImmagine_D.png

0 Kudos
Reply