KDS always performing full build instead of incremental

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS always performing full build instead of incremental

ソリューションへジャンプ
1,394件の閲覧回数
piotrcerba
Contributor III

Hello.

One hour ago I was making changes to my project and everytime I clicked the hammer "Build ... for project" it was performing incremental build, which was always very quick.

Now, suddenly, while clicking this button the environment always performs a full build which in my case takes around 30 seconds.

 

Other projects always build only with incremental build. I don't know what has happened.

 

How to return to the incremental build only setting? What have I done wrong?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,157件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Piotr,

maybe you have renamed your project? I'm aware of such a 'full build' problem if the 'refresh policy' is not correctly set.

See Eclipse Project ‘Refresh Policy’: Broken Incremental Build with External Make? | MCU on Eclipse

Some of the Kinetis SDK v1.2 projects have that problem too, but with the above information there is an easy solution.

I hope this helps,

Erich

元の投稿で解決策を見る

2 返答(返信)
1,158件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Piotr,

maybe you have renamed your project? I'm aware of such a 'full build' problem if the 'refresh policy' is not correctly set.

See Eclipse Project ‘Refresh Policy’: Broken Incremental Build with External Make? | MCU on Eclipse

Some of the Kinetis SDK v1.2 projects have that problem too, but with the above information there is an easy solution.

I hope this helps,

Erich

1,157件の閲覧回数
piotrcerba
Contributor III

Thank you Erich, it helped!

0 件の賞賛
返信