KDS always performing full build instead of incremental

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS always performing full build instead of incremental

Jump to solution
1,488 Views
piotrcerba
Contributor III

Hello.

One hour ago I was making changes to my project and everytime I clicked the hammer "Build ... for project" it was performing incremental build, which was always very quick.

Now, suddenly, while clicking this button the environment always performs a full build which in my case takes around 30 seconds.

 

Other projects always build only with incremental build. I don't know what has happened.

 

How to return to the incremental build only setting? What have I done wrong?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,251 Views
BlackNight
NXP Employee
NXP Employee

Hi Piotr,

maybe you have renamed your project? I'm aware of such a 'full build' problem if the 'refresh policy' is not correctly set.

See Eclipse Project ‘Refresh Policy’: Broken Incremental Build with External Make? | MCU on Eclipse

Some of the Kinetis SDK v1.2 projects have that problem too, but with the above information there is an easy solution.

I hope this helps,

Erich

View solution in original post

2 Replies
1,252 Views
BlackNight
NXP Employee
NXP Employee

Hi Piotr,

maybe you have renamed your project? I'm aware of such a 'full build' problem if the 'refresh policy' is not correctly set.

See Eclipse Project ‘Refresh Policy’: Broken Incremental Build with External Make? | MCU on Eclipse

Some of the Kinetis SDK v1.2 projects have that problem too, but with the above information there is an easy solution.

I hope this helps,

Erich

1,251 Views
piotrcerba
Contributor III

Thank you Erich, it helped!

0 Kudos
Reply