KDS Static Library Project - Bug Report +Fix for future versions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS Static Library Project - Bug Report +Fix for future versions

ソリューションへジャンプ
2,971件の閲覧回数
eli_hughes
Contributor V

There is a bug in KDS V 1.1.0.     I wanted to create a project that builds a static library (CMSIS DSP in this case).   I have done this plenty of times in CW.

 

Process:

 

1.)   I created a KDS project

2.)  I deleted the Startup code

3.) I changed the build artifact to a Static library   C/C++ Build->Settings-->BuildArtifact

 

An error occurs when the archiver is started.   I tracked it down and it turns out that  system build variable "cross_ar" is not defined by default.   Under C/C++ build , build variables I set cross_ar to "ar" and was able to get a project to build.

 

Ideally there should be a nice wizard for static library projects that have this build variable set.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,625件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Eli,

thanks for reporting this! Indeed, this is a problem of the tool chain in KDS. If you switch to library artifact, the Archiver setting is empty.

The correct fix in my view is to specify 'ar' as Archiver, and then it worked for me:

pastedImage_0.png

I have a ticket submitted on this issue so it gets fixed.

thanks,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,626件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Eli,

thanks for reporting this! Indeed, this is a problem of the tool chain in KDS. If you switch to library artifact, the Archiver setting is empty.

The correct fix in my view is to specify 'ar' as Archiver, and then it worked for me:

pastedImage_0.png

I have a ticket submitted on this issue so it gets fixed.

thanks,

Erich

0 件の賞賛
返信
2,625件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Quick update: the issue has been identified, and will be fixed in the next release. Until then, there is the easy workaround to put in 'ar' for the archiever.

I appologize for that problem.

Erich

0 件の賞賛
返信
2,625件の閲覧回数
eli_hughes
Contributor V

Thanks Erich:

I also found this error:

https://community.freescale.com/message/434661#434661

0 件の賞賛
返信