The board is TWR-KE18F, MDK is normal, but in KDS, the system inform Plugin has not been registered. Order the register operation, input my email address , could not register . I had close the firewall .
Can't debug , can't download fash.
Hello Li feng,
- Please first check the Device Manager of PC, is there the OpenSDA driver?
- Please make sure there isn't another connect with your board .
- About the register , Please make your the network is well .
BR
Alice
 
After connect , PC recongised as mbed Serial Port(com5) . How to set it as OPENSDA?
In mdk, set Debug CMSIS-DAP Debugger, work normal, can bulid or download .
Hello Li,
Your board now is MBED firmware, please choose the "GDB OpenOCD debugging":
If it still can't work , please update the bootloader to Jlink or PEMicro.
BR
Alice
Hello Alice,
Now the debugger display is normal, but after debugger or flash download, informed missing a configuration.
 
Whitch is error?
Hello Li Feng,
Please configure the "Config options" as below :
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Alice,
After change config option, run debug, it says the mcu is unsupported.
But I can't find anywhere to change the mcu for import project, how to change it?
Hello Li Feng,
From the error message "MCU is unsupported" , it seems your device is not supported by OpenOCD, as OpenOCD needs to be implemented for your microcontroller. Have you tried P&E and Segger debug firmware on the board
already ? I recommend you test Segger debug firmware, the steps are as below :
1)Press the Reset button (and keep it pressed) while power the board withthe OpenSDA USB connector:.
 2)  The board will show up as BOOTLOADER drive on your system: 
 3) Copy"29_OpenSDA_TWR-KE18F.bin" to the BOOTLOADER driver: 
 4) The copy operation takes about 2-3 seconds, after finished , unpower the board.
 5) Power the board again normally 
Select the "GDB SEGGER J-Link debug" do download and debug :
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Alice,
Think you!
Now I still use MDK, no chanage firmware.
After complete the project, then to find how to use KDS.