KDS Plugin has not been registered

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KDS Plugin has not been registered

1,845 次查看
lifeng
Contributor II

The board is TWR-KE18F, MDK is normal, but in KDS, the system inform  Plugin has not been registered.  Order  the register operation, input my email  address , could not register . I had close the firewall .

001.jpg

002.jpg

Can't debug , can't download fash.

003.jpg

0 项奖励
回复
8 回复数

1,588 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Li feng,

-  Please first check the Device Manager of  PC,  is there the OpenSDA driver?

pastedImage_1.png

- Please make sure there isn't another connect with your board .

- About the register , Please make your the network is well .

BR

Alice

0 项奖励
回复

1,588 次查看
lifeng
Contributor II

pastedImage_1.png pastedImage_3.png

pastedImage_4.png

After connect , PC recongised as mbed Serial Port(com5) . How to set it as OPENSDA?

pastedImage_2.png

In mdk, set Debug CMSIS-DAP Debugger, work normal,  can bulid or download .

0 项奖励
回复

1,588 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Li,

Your board now is MBED firmware, please  choose the "GDB OpenOCD debugging":

pastedImage_1.png

If it still can't work , please update the bootloader to Jlink or PEMicro.

BR

Alice

0 项奖励
回复

1,588 次查看
lifeng
Contributor II

Hello Alice,

Now the debugger display is normal, but after debugger or flash download, informed missing a configuration.

 pastedImage_1.png005.jpg006.jpg007.jpg008.jpg009.jpg010.jpg011.jpg

Whitch is error?

0 项奖励
回复

1,588 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Li Feng,

Please configure the "Config options" as below :

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,588 次查看
lifeng
Contributor II

Hello Alice,

   After change config option, run debug, it says the mcu is unsupported.

pastedImage_1.png

But I can't find anywhere to change the mcu for import project, how to change it?

0 项奖励
回复

1,588 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Li Feng,

From the error message "MCU is unsupported" , it seems your device is not supported by OpenOCD, as OpenOCD needs to be implemented for your microcontroller. Have you tried P&E and Segger debug firmware on the board

already ? I recommend you test Segger debug firmware, the steps are as below :

1)Press the Reset button (and keep it pressed) while power the board withthe OpenSDA USB connector:.
2)  The board will show up as BOOTLOADER drive on your system:
3) Copy"29_OpenSDA_TWR-KE18F.bin" to the BOOTLOADER driver:
4) The copy operation takes about 2-3 seconds, after finished , unpower the board.
5) Power the board again normally

Select the "GDB SEGGER J-Link debug" do download and debug :

pastedImage_1.png


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,588 次查看
lifeng
Contributor II

Hello Alice,

     Think you!

      Now I still use MDK, no chanage firmware.

      After complete the project, then to find how to use KDS.

0 项奖励
回复