KDS Kinetis Bootloader (KBOOT) Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS Kinetis Bootloader (KBOOT) Support

ソリューションへジャンプ
10,604件の閲覧回数
ramstell
Contributor III

The current version of the Bootloader V1.1.0 seems to only support the IAR Toolchain.

 

Are there plans to add support for Kinetis Design Studio?

 

Kind regards

Roger

ラベル(1)
1 解決策
9,801件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Roger,

The Kinetis Bootloader v 1.2.0 will support KDS and is planned to be released next week.

Once it is available you can download it from this page:

Kinetis Bootloader|Freescale

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
14 返答(返信)
9,801件の閲覧回数
a8Chcx
Contributor V

Thanks, Guys.

It works fine now...

0 件の賞賛
返信
9,791件の閲覧回数
a8Chcx
Contributor V

Hi Iva,

I am using KDS 3.0.0 and KSDK 1.2.0 to build FREEDOM K64F Bootloader and found the problem, see attached doc.

Please let me know where the problem can be?

Thanks,

Christie

0 件の賞賛
返信
9,791件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Cristie,

Those errors happen because the project was imported to the workspace with the "Copy projects into workspace" enabled, when you only import the example project to your workspace, then you are leaving the project in its original location in the file system and the links are still valid, but when you "copy" the project to the workspace, only the project folder is copied and not the linked files/resources causing those errors when compiling.

In order to fix the problems you need to delete that project from your workspace and import the example again but this time make sure the "Copy projects into workspace" is not selected:

pastedImage_2.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信
9,791件の閲覧回数
a8Chcx
Contributor V

Hi Gorge/Carlos,

I am using bootloader for FREEDOM K64F project to generate the *.elf and works fine.

Then I use P&E "Debug" to load it into my board, nothing wrong.

But, when I run it, nothing displayed on HyperTerminal. I am using PTB16/PTB17 as my UART port. In this project it says PTA14/15 in bootloader_config.h that I think is wrong.

Could you tell me there is any way to see it is running on UART0? I confirmed that my UART0 is working fine by using another project?

Thanks,

Christie

0 件の賞賛
返信
9,791件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Cristie,

I would recommend you to create a new post for this question on the Kinetis Microcontrollers​ community.

Best Regards!

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信
9,791件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Christie:

Remove the project from the workspace and import it again but DO NOT select "Copy projects into workspace":

pastedImage_0.png

The source and header files are "linked" to the project. If you copy the project then the links are broken.

Regards!

Jorge Gonzalez

0 件の賞賛
返信
9,791件の閲覧回数
a8Chcx
Contributor V

Hi Iva,

I am using MK64FN1M0VLL12 MCU that is the same as FREEDOM K64F platform.

Can I make both development environments available?

Thanks,

Christie

0 件の賞賛
返信
9,802件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Roger,

The Kinetis Bootloader v 1.2.0 will support KDS and is planned to be released next week.

Once it is available you can download it from this page:

Kinetis Bootloader|Freescale

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
9,791件の閲覧回数
a8Chcx
Contributor V

Hi Carlos,

This boot-loader is released? Where can I download it for my K64F?

Thanks,

Christie

0 件の賞賛
返信
9,791件の閲覧回数
DavidS
NXP Employee
NXP Employee

Slight update to release....sorry for delay.

Original date was last week. But we have been fixing a pinmux issue and adding some ease-of-use feature. ETA would be early next week.

Regards,

David

9,791件の閲覧回数
gierdo
Contributor I

Hi!

Are there any news concerning the release of kboot 1.2.0?

Thanks for your info!

0 件の賞賛
返信
9,791件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Dominikus Gierlach,

KBOOT 1.2 we expect in these days, no later than by the end of the week.

I hope this helps,

Iva

0 件の賞賛
返信
9,791件の閲覧回数
a8Chcx
Contributor V

Hi Iva,

The version 1.2 is released. Thank you. I have the following question:

I am using KDS 2.0.0 and KSDK 1.1.0 now.

Do I have to use KDS 3.0.0 and KSDK 1.2.0?

Can I make both development available on the same machine?

Thanks,

Christie

0 件の賞賛
返信
9,791件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Christie Su,

Yes, it is better to use these newest versions.

When you have project developed in KSDK 1.1.0 you should migrate your project to KSDK 1.2 because structure changes greatly.

please what device are you using?

Regards!

Iva

0 件の賞賛
返信