KDS Command Line Clean Build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS Command Line Clean Build

3,193件の閲覧回数
mikewilliams
Contributor I

I'm doing a command line build with KDS.  I followed Erich Styger's guide and I was able to get it to build.  However, I need it to do a "clean" build.  I found the -cleanBuild option but it does a "clean" followed by a "build".  Is there a way to make it just do a clean without building?

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,855件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Mike,

there are only a few options if you run the build with Eclipse on the command line (see https://mcuoneclipse.com/2014/09/12/building-projects-with-eclipse-from-the-command-line/ ).

After the make files have been created, you could run the normal make. See the makefile inside the output (Debug) folder which has the following target:

# Other Targets

clean:

    -$(RM) $(SECONDARY_SIZE)$(OBJS)$(C_DEPS)$(ASM_DEPS)$(SECONDARY_FLASH)$(S_UPPER_DEPS) FRDM-K64F_Demo.elf

    -@echo ' '

so you could call it with

make -f makefile clean

Erich

0 件の賞賛
返信

2,855件の閲覧回数
mikewilliams
Contributor I

I'm gonna plead ignorance so forgive me if I sound dumb. 

If I go to my Build Configuration directory and type 'make clean', it only deletes the .elf file, not the object files.  If I go to KDS and do a 'clean', I see in the console that it deletes the .elf file AND the objects.  Not sure what's going on there.

My goal is to build the project from the command line.  To do that, I used the command from your guide and it works great.  But I can't get it to do a 'clean' only.  To build, I used the build command below:

"c:\My Program Files\freescale\kds_3.0.0\eclipse\eclipsec.exe" -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "..\..\..\KDS Workspaces" -build ATS_ANN_App --launcher.ini "c:\My Program files\Freescale\KDS_3.0.0\eclipse\kinetis-design-studio.ini" --launcher.suppressErrors

I changed -build to -clean, it didn't like that at all.  I changed it to -cleanBuild and it does a clean then a build.  Is there a way to make the above command line do a 'clean' only?

0 件の賞賛
返信

2,855件の閲覧回数
BlackNight
NXP Employee
NXP Employee

call the make file with the clean target:

make clean

This is equivalent to

pastedImage_0.png

Erich

PS: articles on that subject:

https://mcuoneclipse.com/2016/05/26/build-and-clean-selected-files-in-eclipse-cdt/

https://mcuoneclipse.com/2012/02/13/make-my-make-with-eclipse-and-mcu10/

0 件の賞賛
返信

2,855件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello MIKE,

How about the -clean command ?

For Erich have so many guides , could you please tell me which one do you used ?

BR

Alice

0 件の賞賛
返信