KDS 3.0 Builder Makefile changes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS 3.0 Builder Makefile changes

ソリューションへジャンプ
3,070件の閲覧回数
owlsnest
Contributor II

I have a project that I've imported to KDS 3.0 that was written in KDS 2.0. When I try to build the project I run into a compiler error.

 

arm-none-eabi-g++ -mcpu=cortex-m0plus -mthumb -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -T "MKL46Z256xxx4_flash.ld" -Xlinker --gc-sections -L"C:/Users/Todd/KDS/lab2_timer_stopwatch_with_blank/Project_Settings/Linker_Files" -Wl,-Map,"lab2_timer_stopwatch.map" -nanolibc -o "lab2_timer_stopwatch.elf"  ./Sources/slcd.o ./Sources/stopwatch.o  ./Project_Settings/Startup_Code/startup_MKL46Z4.o ./Project_Settings/Startup_Code/system_MKL46Z4.o  

arm-none-eabi-g++: error: unrecognized command line option '-nanolibc'

make: *** [lab2_timer_stopwatch.elf] Error 1

 

After doing some googling it appears that the -nanolibc option should be replaced with --specs=nano.specs --specs=nosys.specs. I open the makefile in KDS 3.0 and make the change to the makefile and save the modified makefile. Then when I go to build the project I get the same error and the make file has been changed back. How do I get the change to the makefile to stay?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,685件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Todd,

the make file is generated. You need to change the linker setting in the project properties. See "Linker Flags for GNU GCC ARM Embedded" in Switching ARM GNU Tool Chain and Libraries in Kinetis Design Studio | MCU on Eclipse .

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,686件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Todd,

the make file is generated. You need to change the linker setting in the project properties. See "Linker Flags for GNU GCC ARM Embedded" in Switching ARM GNU Tool Chain and Libraries in Kinetis Design Studio | MCU on Eclipse .

I hope this helps,

Erich

0 件の賞賛
返信
2,685件の閲覧回数
owlsnest
Contributor II

Erich,

     Thank for your response!

     Under "Project Settings">C/C++ Build>Settings I don't have the "Tool Settings" Tab. Where am I supposed to set the Linker options?

     pastedImage_1.png

0 件の賞賛
返信
2,685件の閲覧回数
owlsnest
Contributor II

I figured it out. That tab is only available if the makefile is automatically generated. Also, if anyone if the future sees this please note the you have to do a make clean (build->clean) before the builder will generate new output files.

0 件の賞賛
返信