KDS 3.0.0 debug level problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS 3.0.0 debug level problem

ソリューションへジャンプ
2,686件の閲覧回数
jimbrady
Contributor I

I recently had a problem with KDS 3.0.0 where the debug level I set in the Debug Level drop-down control for example "Default (-g)", did not get put in the makefile and my .elf executable contained no debug information.  In other words, even though I wanted debug information included in the executable, it was not.  So of course gdb complained that it could not find source code and other things.  When I added "-g" to the  "Other debugging flags" box, then -g was included in the makefile and the .elf file became much larger as expected, and debug was fine.

 

Has anyone seen this ? and any ideas how this could happen ?

 

This problem only happened on a CodeWarrior 10.6 processor expert project I had migrated to KDS 3.0.0.  On a new project created in KDS this problem did not occur.  Am using KDS 3.0.0 on Windows 7. The debug setting I am talking about is in C/C++ Build -> Settings -> Debugging screen.

 

Thanks for the help,

Jim

ラベル(1)
0 件の賞賛
返信
1 解決策
2,505件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jim,

ok, I'm able to reproduce the problem. Indeed, if you have 'none' set in the CW project, somehow the debug level options in KDS project settings are ignored. Seems to be a problem of the CW project converter. I have created a ticket about this.

Thanks for reporting,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,505件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jim,

I have not seen something like this so far, as well not with my converted projects.

So you say it was showing "Default (-g)" in the project options panel, but somehow not used, right?

Maybe there is an inconsitency between what the panel show, and what is actually in the options (in the project file).

Do you know what debug information/option you had in your CodeWarrior project?

Thanks,

Erich

0 件の賞賛
返信
2,505件の閲覧回数
jimbrady
Contributor I

Erich ---

I checked the CW 10.6 project before migrating to KDS 3.0.  Debug level was set to "None".

Yes, I am saying that even though the Debug Level drop-down box says "Default (-g)"  the "-g" is not put in the generated makefile, does not show up in the console messages when building the code, produces a very small executable.elf file, gdb complains there are no debug symbols, can't find source, etc. Putting "-g" into the  "Other debugging flags" box fixes this.

Thanks,

Jim

0 件の賞賛
返信
2,506件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jim,

ok, I'm able to reproduce the problem. Indeed, if you have 'none' set in the CW project, somehow the debug level options in KDS project settings are ignored. Seems to be a problem of the CW project converter. I have created a ticket about this.

Thanks for reporting,

Erich

0 件の賞賛
返信
2,505件の閲覧回数
jimbrady
Contributor I

Erich ---

Thanks for figuring this out.

Jim

0 件の賞賛
返信