K65 Register View

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K65 Register View

1,728件の閲覧回数
Mike_d
Contributor IV

Is there a way to view the K65 registers in KDS in the way CodeWarrior does it?

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,566件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Mike,

yes, but not in the exactly same way, but very similar.

The following articles describes it: https://mcuoneclipse.com/2014/05/29/how-to-add-register-details-view-in-eclipse/ 

That EmbSysRegView is already installed with KDS V3.x (so you don't have to install it), but it describes its usuage if you are not familiar with it.

I hope this helps,

Erich

0 件の賞賛
返信

1,566件の閲覧回数
MarekTrmac
NXP Employee
NXP Employee

Hi Michael,

I have KDS 3.2 installed (in Windows) and I can see the following SVD file on the disk:

c:\Freescale\KDS_v3\eclipse\plugins\org.eclipse.cdt.embsysregview.data_0.2.4.freescale\data\SVD(CMSIS)\Freescale\MK65F18.xml

Can you check on your side?

Regards

Marek

0 件の賞賛
返信

1,566件の閲覧回数
Mike_d
Contributor IV

Hi Erich,

I don't see the K65 in the list.

pastedImage_1.png

0 件の賞賛
返信

1,566件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Michael,

-I think at this time you maybe can not create project about K65.

Please first download  and install the "KSDK_1.3_TWR-K65F180M" , 

download please refer to this thread : How to: install KSDK 2.0 ;

install it to KDS please refer to the DOC under KDS installation directory :KDS_3.0.0\doc\KDS_Users_Guide.pdf

pastedImage_5.png

- Then you can see this chip :

pastedImage_1.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信