Issue porting project to KDS 3.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue porting project to KDS 3.2

1,727件の閲覧回数
denisdantas
Contributor II

Hey there, I installed KDS 3.2, but now I am having an error when trying to compile my project. The header file of some KSDK (1.3.0) files cannot be found now. Do you have any idea what could be causing that?

 

152119_152119.jpgKDS3v2_failure.jpg

ラベル(1)
タグ(2)
2 返答(返信)

1,619件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Denis,

I had this problem with a project once and it was caused because the include paths on the project settings did not have quotation marks, maybe this is the case?

Let me know if it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信

1,619件の閲覧回数
denisdantas
Contributor II

Thank you Carlos, that worked!