Is there PE support for FRDM-KL27Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there PE support for FRDM-KL27Z

ソリューションへジャンプ
3,217件の閲覧回数
snricmn
Contributor II

There is no option for KL27Z on KDSv3 for Processor Expert(also in Kinetis Project v1.2.x) I can only create project with SDKV2.x where there is no processor expert.

Did they drop PE support for KL27Z. Only kl24 25 26 have PE support for kl2.x series

Adsız.png

0 件の賞賛
返信
1 解決策
2,987件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Ahmet

Yes, but it is only supported with SDK 1.3. You need to install the Eclipse update for full board and SDK support in KDS.

Go to Help->install new software->Add->Archive and select the update from the <sdk_1.3>\tools\eclipse_update


Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,988件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Ahmet

Yes, but it is only supported with SDK 1.3. You need to install the Eclipse update for full board and SDK support in KDS.

Go to Help->install new software->Add->Archive and select the update from the <sdk_1.3>\tools\eclipse_update


Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,987件の閲覧回数
snricmn
Contributor II

I downloaded Kinetis SDK 1.3.0 Mainline and Go to Help->install new software->Add->Archive and select the update from the <sdk_1.3>\tools\eclipse_update as you indicated and now under Kinetis 1.X Project or PE Project I can see all boards.

But even if i can start a processor expert project with kl27z now if i choose a pe component like BitIO it says this component is not supported for this mcu. And previously where i was able to do this for kl26z now it cannot be used either i think their support is dropped

0 件の賞賛
返信
2,987件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Ahmet

Yes, as my colleague Erich mentioned PE support has stopped for new parts. So the only way that you can use PE in KL27Z is with SDK components, which does not included components like BitIO.

Best Regards

Jorge Alcala

0 件の賞賛
返信
2,987件の閲覧回数
snricmn
Contributor II

Hi,

Thanks now everything is clear i found that there is sdk component options and they can be used. Complicated than setting registers tho.

Thanks for your answers

0 件の賞賛
返信
2,987件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Yes, PE support has stopped for new parts.

There is way to have some level of Processor Expert for new parts with the Kinetis SDK v2.0, see for example

mcuoneclipse/Examples/KDS/FRDM-KL27Z/FRDM-KL27Z_McuOnEclipseLib at master · ErichStyger/mcuoneclipse... 

I plan to write an article about that approach if there is interest. Basically it is using another device (e.g. KL25Z) to generate code for KL27Z.

Erich

0 件の賞賛
返信
2,987件の閲覧回数
snricmn
Contributor II

Hi Erich

Along with other answer i figured it out. Thanks for your answer.

0 件の賞賛
返信