Is there Kinetis Software Development Kit (KSDK_1.0.0) support for MK60FX512VLQ12 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there Kinetis Software Development Kit (KSDK_1.0.0) support for MK60FX512VLQ12 ?

1,526 Views
thoborawski
Contributor II

We are starting a project with the MK60FX512VLQ12.  I do not see support in KSDK_1.0.0 for this chip. Is there an automated way to generate the

files for a new chip. If not, what would be the best way to approach porting a new chip.  Thanks.

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,402 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Tho,

From the "C:\Freescale\KSDK_1.0.0\doc\Kinetis SDK Release Notes.pfd" , KSDK now do not support MK60FX512VLQ12  .

And as far as  I know , there is no simple way to develop the chips which do not support on SDK so far .

Best Regards,

Alice

0 Kudos
Reply

1,402 Views
adriancano
NXP Employee
NXP Employee

Hi,

The KSDK support for the MK60FX512VLQ12 device will not be available in the next release: KSDK 1.1 targeted for December 2014. But there is a plan to support all legacy devices in future releases.

I hope this information can help you.

Regards,

Adrian

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. It would be nice!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply