Installing FLS_SVD patch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installing FLS_SVD patch

Jump to solution
2,152 Views
pietrodicastri
Senior Contributor II

Good morning

I followed the steps for installing the plug in for KDS, to view the registers. The installation from inside the KDS appears successfull.

I downloaded the patch FSL_SVD_Patch V0.3 for EmbSysRegV0.2.4.zip

from SourceForge. copied the files on the eclipse directory.

Attached the search result in the two directories

19185_19185.pngplugin.png

 

 

 

19188_19188.pngfeatures.png

 

 

 

In the KDS I try to open Window > Preferences > C/C++ > Debug > EmbSys Register View:

 

and I cannot access all the CPU, just one.

19187_19187.pngkdsview.png

 

What to do???

 

Thank You

Labels (1)
Tags (2)
1 Solution
2,019 Views
DavidS
NXP Employee
NXP Employee

Hi Pietro,

I had similar issue but wasn't sure if it was tool related or just me making mistake.

I resolved issue by using the Market Place Update method:

http://mcuoneclipse.com/2014/05/29/how-to-add-register-details-view-in-eclipse/

On that link look for: Alternativly, the menu Help > Eclipse Marketplace can be used. Search for ‘register view':

Then copy-n-paste the contents of the ZIP file/folder "eclipse".

Regards,

David

View solution in original post

2 Replies
2,019 Views
pietrodicastri
Senior Contributor II

Hello David

Thank You for support.

I tried to reinstall using the Market Place.

Just after the recopying of the zip file it is working.

It appears as tool related.

I am happy

Best Regards

0 Kudos
Reply
2,020 Views
DavidS
NXP Employee
NXP Employee

Hi Pietro,

I had similar issue but wasn't sure if it was tool related or just me making mistake.

I resolved issue by using the Market Place Update method:

http://mcuoneclipse.com/2014/05/29/how-to-add-register-details-view-in-eclipse/

On that link look for: Alternativly, the menu Help > Eclipse Marketplace can be used. Search for ‘register view':

Then copy-n-paste the contents of the ZIP file/folder "eclipse".

Regards,

David