Include subfolder KDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Include subfolder KDS

跳至解决方案
2,676 次查看
danielecortella
Contributor V

Hi,

 

i normaly use the method: project properties > c\c++ build > setting > cross arm c compiler > includes for add folder that contain file to build. The problem is that the subfolder aren't include and i have to include all this. There i a better way? i have many subfolder, than add those singly is very long. Thanks

标签 (1)
0 项奖励
回复
1 解答
2,121 次查看
BlackNight
NXP Employee
NXP Employee

Hi Daniele,

unfortunately, that directory structure is not user friendly. It would have been much easier if all the include header files would be a single include folder (as it is standard for other projects). So I'm affraid that you have to add all the folders to the settings. There is no 'recursive' include mechanism in gcc.

Erich

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,121 次查看
BlackNight
NXP Employee
NXP Employee

This trick might be what you are looking for:

Adding Multiple Include Paths to Build Settings in Eclipse | MCU on Eclipse

Erich

2,121 次查看
danielecortella
Contributor V

Hi,

the problem is that i have download this zip: Kinetis Bootloader|Freescale and it contain a src folder with many other folder .... i have to add every subfolder manualy .... There is a faster way for let see the subfolder to the compiler? Thanks

0 项奖励
回复
2,122 次查看
BlackNight
NXP Employee
NXP Employee

Hi Daniele,

unfortunately, that directory structure is not user friendly. It would have been much easier if all the include header files would be a single include folder (as it is standard for other projects). So I'm affraid that you have to add all the folders to the settings. There is no 'recursive' include mechanism in gcc.

Erich

0 项奖励
回复
2,121 次查看
danielecortella
Contributor V

Thanks!

0 项奖励
回复