Migrate from CodeWarrior 16.6 to KDS 2.0.0 problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Migrate from CodeWarrior 16.6 to KDS 2.0.0 problem

Jump to solution
2,284 Views
EarlOrlando
Senior Contributor II

Hi,

 

I'm trying to migrate a project from CodeWarrior to KDS. I tried the steps listed in "C:\Freescale\KDS_2.0.0\doc\pdf\kds_porting_guide.pdf" but when I click in the "Convert CodeWarrior project file..." option, KDS does nothing. I tried reinstalling KDS 1.1.1 without success.

 

Does someone has experimented this problem? Is there another way to migrate the project without start from scratch?

 

FYI, my project has PEx components.

 

Best regards,

Earl.

Labels (1)
1 Solution
1,824 Views
BlackNight
NXP Employee
NXP Employee

Could it be that this project is not a gcc project? The converter will not convert non-gcc projects.

Erich

View solution in original post

2 Replies
1,825 Views
BlackNight
NXP Employee
NXP Employee

Could it be that this project is not a gcc project? The converter will not convert non-gcc projects.

Erich

1,824 Views
EarlOrlando
Senior Contributor II

Oh I see, it is not a gcc project.

Thanks Erich.

0 Kudos
Reply