How to controll results?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to controll results?

跳至解决方案
2,497 次查看
piergiusepperan
Contributor II

Hi, I have to compute some values like current and resistance by software. I mean, I set a particular voltage from 0V to 3.3V ( so from 0 to 65534, for 16 bit) by software on a Digital to Analog Converter, then I want to compute the current, so I define the resistance (for example for 1 ohm resistance, I will write R= 19858, considering 16 bit, i Don't know if it is right) and then I compute the current I= voltage/R; Now, first of all, I don't know if it is possible to compute the current in this way, please, let me know how can I do. The second problem is that I want to verify this result, I mean, i want to veify if the current is right  and I want to see the value of I (the current), on arduino I used the serial port and I wrote printf ("current", I); and i could see the result, is  there a way to see the results on KDS? Thank you

标签 (1)
0 项奖励
回复
1 解答
2,398 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

i think your solution of calculating current is OK.

regarding how to see result with KDS, i suggest you use printf. here is an article for this topic,

How to use printf() to print string to Console and UART in KDS2.0

can this help you?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
2,398 次查看
piergiusepperan
Contributor II

Thank you Peter, I already did like you sugested and It works.

0 项奖励
回复
2,398 次查看
petertoenz
Contributor II

Hello

Your calculation is a bit confusing (for me)

Here ist my way to solve that problem (if you can use float-values):

float R = 1;                                                             // [Ohm]

int16_t U_raw = acd_get_result();                    // replace with your function

float U = (float)U_raw  * ( 3.3 / 2^16 );           // [Volt] (or replace (3.3/2^16) with 0.00005)

float I = U / R;                                                       // [Ampere]

Peter

2,399 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

i think your solution of calculating current is OK.

regarding how to see result with KDS, i suggest you use printf. here is an article for this topic,

How to use printf() to print string to Console and UART in KDS2.0

can this help you?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------