How to configure linker file to use both PFlash and DFlash for .text section on KW36

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to configure linker file to use both PFlash and DFlash for .text section on KW36

1,268 次查看
hagguisouhail
Contributor III

Hello,

I am facing a problem of ".text.ProcessMacCommands' will not fit in region `m_text'". In fact I am using the example of the OTAP client and I want to add to it a LoRa middleware on a kinetis KW36 devboard. I know that the KW36 have 512ko of flash memory split on two bank. However referring to the .ld file of the project, I found that the example uses only one bank (0x00000->0x0003F800). I want to add the second bank (0x10000000->0x100040000) and therfore to split .text region between the two parts. Is there a methos to do this please because the #prgma directive seems not to work with mcuexpresso (warning : ignaoring pragma directive).

0 项奖励
回复
1 回复

1,117 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello

Sorry for the inconvenience this might cause you, but as this product has not been released could you please contact the person who helped you with the access to the information of the product to help you with this question? 

Regards, 

Estephania