How to change the linker file settings for loading the application file into the board ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to change the linker file settings for loading the application file into the board ?

跳至解决方案
2,660 次查看
ganeshramachand
Contributor IV

I am working on MKE02Z64VLD2 controller in KDS 2.0.

150160_150160.jpgLast Nxp Doubt.jpg

The above screenshot is my linker file.

 

150167_150167.jpgLast Nxp Doubt1.jpg

When I load the application S19 file it throws this warning message.

What are the suitable values that should be written in

  1. m_interrupts ?
  2. m_text ?
  3. m_cfmprotrom ?

 

I have attached the application code also.

Original Attachment has been moved to: Application-code.zip

标签 (1)
1 解答
2,210 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ganesh,

    Do you use the UART bootloader  and want to relocate the application address?

    If yes, modify the link file ProcessorExpert.ld,  the m_interrupts Origin = 0x1000,

  m_data = 0x1000, length = 0xfbf0-0x1000;

m_cfmprotrom don't need to modify.

About the detail relocate address, you can check your bootloader code,

#define RELOCATION_VERTOR_ADDR 0x1000

Besides, your KDS version is to low, you can go to : www.nxp.com/kds download KDS3.2.

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
2,211 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ganesh,

    Do you use the UART bootloader  and want to relocate the application address?

    If yes, modify the link file ProcessorExpert.ld,  the m_interrupts Origin = 0x1000,

  m_data = 0x1000, length = 0xfbf0-0x1000;

m_cfmprotrom don't need to modify.

About the detail relocate address, you can check your bootloader code,

#define RELOCATION_VERTOR_ADDR 0x1000

Besides, your KDS version is to low, you can go to : www.nxp.com/kds download KDS3.2.

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,210 次查看
ganeshramachand
Contributor IV

Thanks alot. I fixed that problem. Now I dont know how to load my own application file into the boot loader. Can u kindly check out this thread and reply. How to run the application file in the Freescale Universal boot loader ?

0 项奖励
回复
2,210 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ganesh,

    We will help you to answer that question in your new post!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------