How to add linked files in KDS V1.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to add linked files in KDS V1.1

跳至解决方案
1,758 次查看
randylee
Contributor V

IN CW 10.5 just under the import/exprort items in the context menus of the project or source directory, there is an "add files" which is where I can simply add files to the project and link files that I want noticed from elsewhere.

 

In KDS V1.1 There is no such option only import file file system and that doesn't let you link the file (i.e. just include it in the project without messing with it).

 

I see linked files in projects typically in the directory "Static_Code" so I know Elclipse hasn't forgotten how to do it, but I can't for the life of me find the majical incantation to just have it do it.

 

Any hints?

标签 (1)
0 项奖励
回复
1 解答
1,285 次查看
BlackNight
NXP Employee
NXP Employee

Here are multiple ways and hints:

Link to Files and Folders in Eclipse | MCU on Eclipse

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,285 次查看
randylee
Contributor V

yep, that got it.... thanx!

0 项奖励
回复
1,286 次查看
BlackNight
NXP Employee
NXP Employee

Here are multiple ways and hints:

Link to Files and Folders in Eclipse | MCU on Eclipse

I hope this helps,

Erich

0 项奖励
回复