How to add linked files in KDS V1.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add linked files in KDS V1.1

ソリューションへジャンプ
1,660件の閲覧回数
randylee
Contributor V

IN CW 10.5 just under the import/exprort items in the context menus of the project or source directory, there is an "add files" which is where I can simply add files to the project and link files that I want noticed from elsewhere.

 

In KDS V1.1 There is no such option only import file file system and that doesn't let you link the file (i.e. just include it in the project without messing with it).

 

I see linked files in projects typically in the directory "Static_Code" so I know Elclipse hasn't forgotten how to do it, but I can't for the life of me find the majical incantation to just have it do it.

 

Any hints?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,187件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Here are multiple ways and hints:

Link to Files and Folders in Eclipse | MCU on Eclipse

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,187件の閲覧回数
randylee
Contributor V

yep, that got it.... thanx!

0 件の賞賛
返信
1,188件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Here are multiple ways and hints:

Link to Files and Folders in Eclipse | MCU on Eclipse

I hope this helps,

Erich

0 件の賞賛
返信