How do you display port and module registers in Kinetis Design Studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do you display port and module registers in Kinetis Design Studio

1,412件の閲覧回数
Kenm
Contributor II

How do you display port and module registers in Kinetis Design Studio?  So they can be changed

Are these registers in the configuration registers?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,173件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Ken,

you need to install an additional plugin.

See

http://mcuoneclipse.com/2014/05/29/how-to-add-register-details-view-in-eclipse/

Then apply the V0.3 patch from SourceForge which has the Freescale CMSIS-SVD files in it from McuOnEclipse - Browse /Eclipse Plugins/EmbSysReg at SourceForge.net

I hope this helps,

Erich

0 件の賞賛
返信

1,173件の閲覧回数
jinxin_cn
Contributor I

Hi Erich,

I can't find the chip KV31F51212 in V0.4 patch. How could I do?

B.R.

Jin Xin

0 件の賞賛
返信

1,173件の閲覧回数
BlackNight
NXP Employee
NXP Employee

You could use the files from Kinetis Design Studio v3.0.0:

pastedImage_0.png

?

Erich