How can I select KL03z in Processor Export in Kinetis Design Studio v1.3.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I select KL03z in Processor Export in Kinetis Design Studio v1.3.0

2,193 Views
perf
Contributor I

I'm a beginner with Kinetis design Studio. I have a FRDM-KL03z board and want to use Processor expert when I develop code. But when I have setup a project with KL03z as target then i can't find it in processor expert. How can I do that?.

 

I can see KL02z and KL04z but not KL03z.

 

Best Regards,

Per

Labels (1)
0 Kudos
Reply
3 Replies

1,947 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

The KSDK 1.3 mainline release contain the support of the KL03. See the following link:

 

http://www.nxp.com/products/wireless-connectivity/2.4-ghz-wireless-solutions/ieee-802.15.4-plus-ble/...

 

and navigate to the Kinetis SDK 1.3 Mainline download link:

 pastedImage_1.png

To work with KL03+processor expert, we need:

1. install KDS3.2

2. install KSDK1.3 mainline.

3. Do update from KDS IDE menu "help", "check for update".

then you will see KL03 and processor expert available. see attached video.

 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,947 Views
DavidS
NXP Employee
NXP Employee

Hi Per,

Please goto the Freedom frdm-kl03 product page at following link:

FRDM-KL03Z|Freedom Development Platform|Kinetis MCU|NXP

Click the Getting Started tab and follow instructions to setup tools and run examples from KSDK_1.3.

Note KSDK_1.3 will work with PE in KDS.  But newest KSDK_2.0 does not support PE.  So when installing tools make sure you install the KSDK_1.3.

Then for working with PE look here:  How to start with KSDK

Regards,

David

PS

For those that want to use KSDK_2.0 without PE the support is coming in June:

Introducing Kinetis SDK v2

0 Kudos
Reply

1,947 Views
kalamlee
Contributor I

Dear David

actually, I confront to the same problem. I have followed your instructions and watched the video. The KL03 is missed.

I only see KL02z and KL04z but not KL03z when I create the new project to choose the processor!

Would you help me ???

Regards,

Ka Lam

0 Kudos
Reply