Removing debug info

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Removing debug info

2,715件の閲覧回数
davidsherman
Senior Contributor I

Seeing something that seems like I'm doing the right thing, but I'm not.  We're bumping into flash size limitations, and according to the map file, there is debug info in places (for example, .debug_macro, .debug_ranges).  In the debugging settings under the project properties I can change from maximum to none, and the debug sections are gone from the map, but the ROM image is exactly the same size.  Am I missing something?  We do have size optimization turned on.  Can we remove the debug info to make it smaller?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,631件の閲覧回数
BlackNight
NXP Employee
NXP Employee

David,

debug information does not count for code size, it does not get programmed/downloaded into the target, see Debug vs. Release? | MCU on Eclipse .

You can check your actual code size with the 'size' utility (see Code Size Information with gcc for ARM/Kinetis | MCU on Eclipse  and text, data and bss: Code and Data Size Explained | MCU on Eclipse .

There are several other options (including -Os) which affect code size.

Or what you are using from the libraries: e.g. not using printf() and the like can reduce your code size by 10-20 kByte depending on usage. There -Lto (Link time Optimization) which optimizes across compilation units which can have a positive impact too.

I hope this helps,

Erich

0 件の賞賛
返信

2,631件の閲覧回数
davidsherman
Senior Contributor I

Thanks Erich, we managed to free up space.  I had forgotten that kernel logging was still turned on for MQX-Lite.  We did look into the link-time optimization, but down in the guts of the MQX-Lite kernel turning that on created some alignment problems that led to run time errors.

0 件の賞賛
返信