Grouping components in KDS(processor expert)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Grouping components in KDS(processor expert)

1,196件の閲覧回数
arunkumar1989
Contributor I

Hello,

Is it possible to group a set of components in KDS?

 

For example ,if i have an SPI_MasterLDD and a couple of Bit IOs LDD,can i group them into one and later if i add the group the same components with the same settings can be used in any future projects?

Note:I do not want to create a new component all together,just to group them into one single unit.

I really like processor expert ,but it would be really helpful if there was a simple button to do this.

Just select all the components you want to group(in the components view),right click and there should be an option "group" or something similar.

 

In code warrior ,we have a similar setting.When you right click on the component we get an option "Save component settings as template" which is missing in KDS

 

Thanks in advance,

Arun

ラベル(1)
0 件の賞賛
返信
1 返信

1,131件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

you can put components into groups/folders. Create a group/folder with the context menu:

pastedImage_0.png

Use File > Export to export component settings:

pastedImage_1.png

See Export and Import Processor Expert Component Settings | MCU on Eclipse

I hope this helps,

Erich

0 件の賞賛
返信