Grouping components in KDS(processor expert)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Grouping components in KDS(processor expert)

1,168 Views
arunkumar1989
Contributor I

Hello,

Is it possible to group a set of components in KDS?

 

For example ,if i have an SPI_MasterLDD and a couple of Bit IOs LDD,can i group them into one and later if i add the group the same components with the same settings can be used in any future projects?

Note:I do not want to create a new component all together,just to group them into one single unit.

I really like processor expert ,but it would be really helpful if there was a simple button to do this.

Just select all the components you want to group(in the components view),right click and there should be an option "group" or something similar.

 

In code warrior ,we have a similar setting.When you right click on the component we get an option "Save component settings as template" which is missing in KDS

 

Thanks in advance,

Arun

Labels (1)
0 Kudos
Reply
1 Reply

1,103 Views
BlackNight
NXP Employee
NXP Employee

Hello,

you can put components into groups/folders. Create a group/folder with the context menu:

pastedImage_0.png

Use File > Export to export component settings:

pastedImage_1.png

See Export and Import Processor Expert Component Settings | MCU on Eclipse

I hope this helps,

Erich

0 Kudos
Reply