Group S19 image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,183件の閲覧回数
arnogir
Senior Contributor II

Hello

 

In many application I have based on Kinetis, In production phase, I have to flash with the P&E the USB bootloader and then with the boot, insert the USB key containing the programme S19 image which will flash it and jump to it.

 

So I have two programme in the flash (Boot + Application)

Are they a way to create a unique flash image containing both program? In other word, can we merge 2 s19 (or Abs) file in only one?

 

By this way, in production phase, the second step which consist to flash the application with USB bootloader will be not necessary.

 

thank you

ラベル(1)
0 件の賞賛
返信
1 解決策
2,032件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

please refer Erich's article as below

https://mcuoneclipse.com/2016/02/26/merging-s19-files/

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,032件の閲覧回数
arnogir
Senior Contributor II

Light, fast, efficient, my personal research had not given anything!

Thank for your help, I think the link is what I research.

:smileyhappy:

0 件の賞賛
返信
2,032件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

Best Regards,

Jennie Zhang

0 件の賞賛
返信
2,033件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

please refer Erich's article as below

https://mcuoneclipse.com/2016/02/26/merging-s19-files/

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信