Generating code for K10 2N30D?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generating code for K10 2N30D?

Jump to solution
1,988 Views
d_m_d
Contributor I

Is there an option to generate code in KDS3.0.0 for PK10N512VLL100 2N30D (Revision 1.2)?

Selection of MK10DN512VLL10 100LQFP (which is the closest match) is generating code accessing registers (like RCM) only supported in Revision 2.

If not directly supported, is there any recommended workaround?

 

Update:

- Disabled Internal Peripherals/Reset Control suppresses the unwanted RCM register accesses

- Removed Watchdog

- Commented out MCG_C7 access

This allows user code to be reached, but hand editing seems to be unavoidable as other clocking modes and peripherals are added (according to AN4445 including RTC/TSI ...)

Labels (1)
1 Solution
1,915 Views
d_m_d
Contributor I

Confirmed - Thank You

View solution in original post

0 Kudos
Reply
2 Replies
1,916 Views
d_m_d
Contributor I

Confirmed - Thank You

0 Kudos
Reply
1,915 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello,

PK10N512VLL100 is the prequalified partnumber of the MK10DN512ZVLL10, so you should create a project for the MK10DN512Zxxx10

Regards,

Santiago