Generate makefile for linux with KDS for KW40/41

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generate makefile for linux with KDS for KW40/41

1,553 Views
sensenthuran
Contributor IV

Hi,

 

How to generate a makefile for Linux build machine from KDS for KW40/41 application (say hci_app)?

 

Thanks

Labels (1)
0 Kudos
Reply
2 Replies

1,286 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

In addition, Makefile is automatically generated after a successful build under the same folder with .elf file.

user can edition makefile style and syntax in KDS preferences window.pastedImage_0.png

pastedImage_1.png

Hope this helps!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,286 Views
MarekTrmac
NXP Employee
NXP Employee

Hi,

just select Build command in the menu. Makefile is created automatically in Debug folder.

Regards

Marek

0 Kudos
Reply