Flashing KBOOT and Initial App

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flashing KBOOT and Initial App

跳至解决方案
1,594 次查看
alex323qp
Contributor III

Hi everyone, I'm trying to flash a custom bootloader based on the KBOOT 1.2 and also an initial app to my target KL25Z64 through KDS, using the PEMicro Universal Multilink FX. I'm first flashing the base app (with the right start location) and then the bootloader (.elf files), but it looks like on every flashing the previous binary gets replaced, is there any "right" procedure I'm not following?

 

p.s I also tried unchecking the "Mass erase on connect" checkbox without success.

107695_107695.pngpastedImage_0.png

 

Thanks in advance,

 

Alex.

标签 (1)
0 项奖励
回复
1 解答
1,196 次查看
alex323qp
Contributor III

The answer was right under my nose:

For those that may have the same question, you can "Preserve" Memory ranges from the "Advanced Options" button.

More information here: preserved memory range problem in KDS 3.0

Cheers,

Alex.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,197 次查看
alex323qp
Contributor III

The answer was right under my nose:

For those that may have the same question, you can "Preserve" Memory ranges from the "Advanced Options" button.

More information here: preserved memory range problem in KDS 3.0

Cheers,

Alex.

0 项奖励
回复